Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do you connect serially to a PLC with Concept via a TSXETG100 Ethernet to Modbus Gateway?

Issue:

How do you connect serially to a PLC with Concept via a TSXETG100 Ethernet to Modbus Gateway?

Causes and Fixes

The first thing that needs to be done is to add the Modbus address of the PLC into the Device list of the TSXETG100.
To do this Log into the TSXETG100 through Internet Explorer by typing in its IP address and entering a Username and Password (the defaults are Administrator with a password of Gateway).
Connect

After Logging in chose Setup, then Device List, and add the Modbus address of the PLC to the Device List and hit Apply.

Internal web page

Launch Concept, open your project chose Connect from the Online Menu.

Connect

For a Protocol chose TCP/IP, type in the IP address of the TSXETG100 and the index ( Modbus address) of the PLC. Then hit OK to connect to the PLC.

PLC connection

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)