Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I log data to a USB storage device with the Magelis XBT-GT1005 and XBT-GK series?


Vijeo-Designer 4.6.0 supports external USB storage drives for storing runtime-generated data, including Data Logging files.

In Vijeo-Designer, at the target level, the property called "Data Locations" indicates where to store the files. What is new in Vijeo-Designer 4.6.0 is that the "Optional Drive" is possible to select in the "Data Locations" window for the following targets:
- XBTGT Series targets.
- XBTGK Series targets.
- XBTGT1005 Series targets.