Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the default IP address for the M340 MB+ proxy TCSEGDB23F24FA?

The default IP address can be found by converting the last 2 numbers of the MAC address from Hex to Dec and preceding them with 85.16

Example:
MAC address 00.80.F4.06.4C.38
4C Hex converts to 76 Dec
38 Hex converts to 56 Dec

Default IP address is 85.16.76.56


Legacy KB System (APS) Data: RESL198530 V1.0, Originally authored by MiMe on 05/18/2009, Last Edited by MiMe on 05/18/2009
Related ranges: Modbus Plus