Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Video: How to create and save a Data Watch Window in the ProWORX 32 v2.1 programming software.

Goals and Symptoms

To create and save a Data Watch Window in the ProWORX 32 v2.1 programming software.

Causes and Fixes

The following video demonstrates how to create, then save a Data Watch Window for registers 40030 through 40035. A written procedure is available below the video.



There are two ways to open a Data Watch Window. You can either.....
1- Go to the main toolbar and select PROJECT then DATA WATCH WINDOW.
or
2- From the Navigation window, open DATA EDITORS and select DATA WATCH WINDOW.

img1

Once the Data Watch Window has been opened, follow this procedure for filling the Data Watch Window with addresses:
1- Right-click in the Data Watch Window, and click Fill Addresses. The Add Addresses dialog box opens.
2- Enter address 40030 in the Starting Address field. This is the first in a range of addresses to be added to the Data Watch Window.
3- Enter numeric value 6 in the Number of Addresses field. This is the length of the range of addresses (40030 to 40035) to be added to the
Data Watch Window.
4- Click OK. Addresses specified are added at the current grid location. Existing addresses may be overwritten.

img2

To save the Data Watch Window template, right-click in the Data Watch Window, and click Save Address Template.
A Datawatch Log File (*DWA) will be created with the project name and placed into the folder you choose.
img3

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings