Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Will the ATV61HC11N4T1 ship with a DC choke?
Issue:
Does ATV61HC11N4T1 comes with a DC choke?

Product Line:
Altivar 61, Altivar 71

Environment:
ATV61/ATV71HD55M3X-HD90M3X, ATV611HD90N4-HC63N4, ATV71HD90N4-HC50N4.  (including T1 and/or S383 suffix)

Cause:
Is the DC Choke included or does it need to be ordered separately and if so, what is the part number?

Resolution:
The part numbers listed above do require an external DC choke.  This DC choke is included with the drive when ordered and does not need to be ordered separately.  It does ship separately though.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings