Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
CM2000 Alarm and Event Setpoint Selection

Issue:
Customer wants to configure alarm and event alarms

Product Line:
CM2000 Series Meters

Environment:
Alarm and Event Setpoint Selection

Cause:
The CM2000 series meters has onboard alarms and events that can be configured. There are 4 setpoint settings for each alarm/event: Pickup Value, Pickup Delay, Dropout Value, and Dropout Delay.

The Pickup and Dropout values can be chosen as a certain percent above or below the nominal value for that measurement.

Resolution:
The attached spreadsheet can be used to help determine the desired pickup and dropout values for voltage related alarms/events based on the nominal voltage and the desired pickup and dropout %.

For example, alarm 16 is an overvoltage alarm. If the desired pickup value is 105% of the nominal voltage and the nominal voltage is 480V, the pickup value would be 504V. If the desired dropout value is 95% of the nominal voltage, the dropout voltage would be 456V.

*For information on configuring alarms from the front panel check out Video: Alarm and Relay Setup for the CM2000 Series Meter from the Front Panel

Schneider Electric Nigeria

Attachment(s)
Alarm and Event Setpoint Helper.xls.xlsx [11.59 KB]