Issue
Customer is looking for datasheet for Class 4210 Voltage and Current transformers.
Product Line
Class 4210 Transformers
Cause
Customer is looking for datasheet for Class 4210 Voltage and Current transformers.
Environment
Datasheet and specification for Class 4210 Transformers.
Resolution
The datasheet for Class 4210 Transformers are attached below.
These part numbers and document are for reference only. The devices are Legacy Transformers no longer sold by SE.
Released for: Schneider Electric Nigeria
Discontinued
Discontinued
Discontinued
Discontinued