Powerlogic/ION meter comparison chart (Internal)
Issue
A user may want to compare features between different meters from different manufacturers
Product Line
Meters - iEM 2000/iME, iEM 3000 series, BCPM, EM4000 series, PM8000 series, PM5000 series, ION6200, PM210, PM600 series, PM700 series, ION6200, ION7300 series, ION8800, ION8650, ION8600, CM2000 series, CM3000 series, ION7550/ION7650, CM4000 series
Environment
Metering and Power Monitoring
Cause
A user may want to make comparisons between Schneider meters and meters from other manufacturers
Resolution
- If making a comparison between Schneider meters only, the current offer comparison chart may be found at the link below:
https://www.pmutraining.com/files/meter-selection-guide.pdf
- For competitor comparisons, please reference the attached excel file (12959.xls).
Released for: Schneider Electric Nigeria