How can we help you today?

ION 8650 Modbus and DNP values do not scale correctly

Issue
Scaling of DNP and Modbus output values may be incorrect when the PT ratio is set at 1:1. This will turn on the Scaled Operational Values output prematurely. It should only be enabled when BOTH the PT AND CT ratios are set to 1:1.
ION8650 Variant A

    • - 8650A_RMICAN_35S_V4.1.0.0.5.dcf
      - 8650A_RMICAN_V4.1.0.0.5.dcf
      - 8650A_V400_FAC-35S_V4.1.0.0.2.dcf
      - 8650A_V400_FAC_V4.1.0.0.2.dcf
      - Any framework derived from the above frameworks, including all prior revisions.
ION8650 Variant B
    • - 8650B_RMICAN_35S_V4.1.0.0.5.dcf
      - 8650B_RMICAN_V4.1.0.0.5.dcf
      - 8650B_V400_FAC-35S_V4.1.0.0.2.dcf
      - 8650B_V400_FAC_V4.1.0.0.2.dcf
      - Any framework derived from the above frameworks, including all prior revisions.
ION8650 Variant C
    • - Is not affected

Product

ION8650A

ION8650B

ION8650C

Enviorment

ION Meters

Cause
An incorrect formula is populated within the Arithmetic 74 (SetRatios1) formula 1 for the A and B variants (C variant is correct).
The incorrect formula on Variant A and B is IF(S1=S2,1,0), which can be seen below.

formula

Resolution
The corrected formula can be seen below as IF(AND(S1=S2,S3=S4),1,0)
formula corrected

The fix to this formula can be done directly in unlocked meters using IONSetup or Designer, or download the corrected template listed below.

These formulas have been fixed in:

ION8650 Variant A

    • - 8650A_RMICAN_35S_V4.1.0.0.6.dcf
      - 8650A_RMICAN_V4.1.0.0.6.dcf
      - 8650A_V400_FAC-35S_V4.1.0.0.3.dcf
      - 8650A_V400_FAC_V4.1.0.0.3.dcf
      - Any framework derived from the above frameworks.
ION8650 Variant B
    • - 8650B_RMICAN_35S_V4.1.0.0.6.dcf
      - 8650B_RMICAN_V4.1.0.0.6.dcf
      - 8650B_V400_FAC-35S_V4.1.0.0.3.dcf
      - 8650B_V400_FAC_V4.1.0.0.3.dcf
      - Any framework derived from the above frameworks.
ION8650 Variant C
    • - Is not affected

Schneider Electric Nigeria
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
Need help?

Need help?

Product Selector

Product Selector

Quickly and easily find the right products and accessories for your applications.

Get a Quote

Get a Quote

Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Centre

Help Centre

Find support resources for all your needs, in one place.
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings