Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
170ANR1209x Discrete Inputs Oscillate On/Off Under Certain Conditions

Issue
The purpose of this Resolution is to inform users of 170ANR12090 and 170ANR12091 Momentum I/O Bases of a problem with the discrete input data oscillating on and off, although no input signals are present.

The discrete input bits (lower byte of input word 2) will continuously oscillate on/off when at least one of the inputs is turned on from the field side. This occurs if the parameters for the analog outputs are set to either of the following two configurations:

When User Defined Value is selected for Channel 3 and the value is set greater than 255 decimal or 100 hex. (4x I/O map word #6)
When User Defined Value is selected for Channel 4 and the value is set to any number other than zero. (4x I/O map word #7)

The other 2 analog output parameter selections, Minimum Output, and the default parameter Hold Last Value, do not produce this condition.


Product Line
170ANR12090
170ANR12091


Resolution
A firmware solution has been implemented. Modules with an SV of 1.10 and a PV02 have this fix.

This is not a field upgradable option. Applications using this module that are experiencing discrete inputs issues using the above-mentioned parameters may be exchanged under warranty. With the parameter settings described, the problem will occur when a discrete input is made active. Parameter settings other than those described above will not exhibit this problem.


Legacy KB System (APS) Data: RESL164637 V3.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum I/O

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings