Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to update multiple loadables in ProWORX NxT

Goals and Symptoms

How to update multiple loadables in ProWORX NxT

Facts and Changes

All versions of ProWORX NxT

Causes and Fixes

'ProWORX NxT' does not allow the update of multiple loadables at the same time. If more than 1
loadable needs to be updated, the update must be performed one at a time.

The following example updates the ESI loadable which also includes the NSUP loadable.

  • Open the project.
  • Click on 'Configuration' from the top menu bar and select 'Configuration'.
Configuration
  • Click on 'User Loadables'
  • Click on first loadable to be updated (i.e., NSUP) in the Loadables in database window.
  • Click on the Update button.


Controller configuration
  • Find the the executable file (i.e., NSUP.exe) and select it.
  • Click on the OK to close the Select Loadable File window.
Loadable file selection
  • Click on the OK in the 'Update Successful' message box.
Ok window
  • Click on the OK to save the changes and to close the Controller Configuration window.
  • Repeat the process to update the next loadable. (i.e., ESI)