Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Momentum Processor Run LED May Blink 2x with an Crash Code 836 After a Power Cycle

Issue
This resolution describes a potential issue where the Momentum PLC RUN LED blinks in an error pattern after a power cycle.

A Momentum PLC Run LED may blink 2x with a crash code 836 after the Momentum assembly is power cycled. The same error may also occur if the Momentum PLC is in RUN mode (without a power cycle event). This condition may occur only if a 172PNN2x022 or 172JNN21032 is part of the assembly. The error will not occur if the 172PNN2x022 or 172JNN21032 is removed or not part of the assembly.


Product Line
Momentum


Resolution
This resolution affects the following adapters with the PV number and the 'Date of Manufacture' (DOM) listed:
The PV and DOM numbers are found on the battery access door of the PNN and JNN adapters.

Part Number
PV number
Date of Manufacter (DOM)
172JNN21032
PV01 or lower
0801 or higher
172JNN21032C
PV02 or lower
0801 or higher
172PNN21022
PV04 or lower
0801 or higher
172PNN21022C
PV03 or lower
0801 or higher
172PNN26022
PV04 or lower
0801 or higher

Changes were made to optimize filtering on the power supply circuit to improve power on and runtime stability. These changes are not field upgradeable.

If the Momentum PLC Run LED is exhibiting the symptoms described above, it is recommended that the 172PNN2x022 or 172JNN21032 be exchanged. If an exchange is necessary, reference the Quality Information document IQ102452 when ordering.

The following PV numbers identify new or updated adapters

Part Number
PV number
Date of Manufacter (DOM)
172JNN21032
PV02 or higher
does not apply
172JNN21032C
PV03 or higher
does not apply
172PNN21022
PV05 or higher
does not apply
172PNN21022C
PV04 or higher
does not apply
172PNN26022
PV05 or higher
does not apply



Legacy KB System (APS) Data: RESL203517 V1.0, Originally authored by DaDz on 09/23/2010, Last Edited by DaDz on 09/23/2010
Related ranges: Modicon Momentum

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings