Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
140NOC77101 Explicit Messaging CIP Modbus Object Read Example

Issue
The attached document is a CIP Modbus Object Read example for a 140NOC77101 using the MBP_MSTR block to read from another Quantum 140NOC77101.


Product Line
Quantum
140NOC77101


Resolution
This program will read from located registers in Schneider PLC's with the following network modules installed:

  • 140NOC77101
  • BMXNOC0401
  • TSXETC101

Do not use this example to read from located registers in Schneider PLC's through the following network module:
  • 140NOC78000

Attachments
170NOC77101_CIP_Modbus_Object_READ_Example.pdf

Schneider Electric Nigeria

Attachment(s)
170NOC77101_CIP_Modbus_Object_READ_Example.pdf [166.68 KB]