Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is MTBF (Mean Time Between Failures) Calculated?

1. Computed following RDF2000 Reliability model (UTE C 80-810 standard) - EQUIPMENT ambient temperature at 30deg C (86deg F), 60deg C (140deg F) and 85deg C (185deg F)

2. Continuous operation profile: 100% operation rate per year (365d / year, 24h / day) - 12 power on/off per year (1 per month) - No stocking days

3. Intermittent operation profile: 46% operation rate per year (335d / year 12h /day) - 335 power on/off per year (1 per operating day) 30 stocking days

4. MTBF are given in hours