Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do ION meters use IEEE 802.3 or Ethernet Type II TCP framing?

ION communication protocol over Ethernet median uses IEEE 802.3 type TCP framing.

  • Date Created: July 24, 2008
    Last Revised: February 20, 2009
    Public
    Original Author: KG
    All content © 1992-2009 Schneider Electric

Legacy KB System (APS) Data: RESL197866 V1.0, Originally authored by KBAdPM on 02/21/2009, Last Edited by KBAdPM on 02/21/2009
Related ranges: ION8600, ION7550/ION7650, ION7300