Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do ION meters support UDP (User Datagram Protocol) via the ethernet port?

Issue

Can you use UDP (User Datagram Protocol) via the ethernet port in ION meter

Product Line

ION meters

Environment

Communication protocol

Cause

User want to know if the meter can setup UDP via Ethernet.

Resolution

ION meters do not support UDP. The ION meters do however support Modbus TCP (port 502), ION protocol over TCP, and Modbus RTU over TCP.