Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Momentum I/O Base Ground Stud.

Issue
The purpose of this resolution is to inform Momentum I/O Base users of a potential ground stud issue affecting the product.  During assembly, the screw which is used to secure a ground wire lug, was tightened beyond manufacturing specifications.


Product Line
Momentum



Resolution
On rare occasions, the solder connection of the I/O Base ground stud may break when loosening or tightening the ground stud screw.


Modules affected:

  • All I/O Base model numbers.
  • This issue may occur on I/O Base modules built before Aug. 2004 with a serial number of 210431xxxxx or less.
    Modules not affected:
    • Modules with a serial number of 210431xxxxx and less with an 8-2004 label on the back of the modules have been inspected and are ok.
    • Modules with a serial number greater than 210431xxxxx are ok.

Legacy KB System (APS) Data: RESL166464 V1.0, Originally authored by on , Last Edited by on
Related ranges: Modicon Momentum I/O

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings