Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the inrush current of the ATV61 High horse power VFDs?
Issue:
Inrush current of the ATV61 / ATV71 High horse power VFDs.

Product Line:
ATV61HC11N4,  ATV61HC31N4, ATV61HC25N4,  ATV61HC40N4,  ATV61HC63N4
ATV71HD90N4, ATV71HC20N4,  ATV71HC25N4,  ATV71HC31N4,  ATV71HC50N4

Environment:
All

Cause:
Application requirement.

Resolution:
Inrush current
Drive power  [kW]             I peak [A] (~2ms)                  I peak [A] (~2ms)
ATV71    ATV61               @ 480V +10%                        @ 400V
90               110                   275                                        208
200             250                   556                                        421
250             315                   764                                        579
310             400                   802                                        608
500             630                  1500                                     1136