Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to open an ICD, CID, or SCD file with CET850

Issue
Unable to open ICD, CID, or SCD file using the CET850 software

Product Line
CET850

Resolution
Use the attached document as a guide to opening any ICD, CID, or SCD file using the CET850 software. Access the CET850 software through the following link: CET850 IEC 61850 configuration tool V4.13.0 | Schneider Electric.

Schneider Electric Nigeria

Attachment(s)
Opening files with CET850.pdf [272.36 KB]
CET850-V4.13.0.zip [210.68 MB]