Issue:
Trying to program R1 and R2 relays, on the ATV61 or ATV71 drives.
Product Line:
Altivar ATV61 and ATV71
Environment:
All
Cause:
Relay program assignment
Resolution:
Under the DRIVE MENU, select Menu 1.5 INPUTS / OUTPUTS.
Scroll down and select R1 CONFIGURATION.
Select R1 Assignment, and then select the desired function, such as No drive flt, Drv running, etc...
The same can be done for R2 CONFIGURATION.
Released for: Schneider Electric Nigeria