Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use R_TRIG, F_TRIG, TRIGGER, TON, TOFF, and TP function blocks in Section 0 of a Unity / Quantum HotStandby system?

Issue:
R_TRIG, F_TRIG, TRIGGER, TON, TOFF, and TP function blocks usage in first PLC section


Product Line:
Quantum HSBY


Resolution:
No. R_TRIG, F_TRIG, TRIGGER, TON, TOFF, and TP function blocks cannot be used in Section 0 (First PLC section) of a HSBY system because their use can lead to unintended changes in state at switchover. Section 0 is the only section solved by a Standby System and is updated at the end of scan by the Primary.


Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings