Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the default directory for ICD files installed with the SFT common library?

Issue
Need the default ICD file for a SEPAM relay.

Product Line
CET850
ICE61850

Resolution
The default directory is as follows:

Install drive (Typically C) > Program Files (X86) (Only X86 if installed on a 64-bit operating system) > Schneider > SFTCommon > IEC61850 > Edition_1 > ICD

This directory contains all of the ICD files that CET850 contains.