Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it possible to have two different versions of Vijeo Designer Installed on a PC?
Issue
Is it possible to have two different versions of Vijeo Designer Installed on a PC?

Product Line
Vijeo Designer

Resolution
It is only possible to have Vijeo Designer V6.2 and one version older (for example v6.1 or v6.0).
  1. Install the earlier version first.
  2. Then install the newer version.
  3. When prompted if you want to replace older version with newer version, choose [No]"

Note Install folders for each version are as follows:
For versions older than 6.2: "C:\Program Files (x86)\Schneider Electric\Vijeo-Designer\"
For version 6.2, the installation folder will be: "C:\Program Files (x86)\Schneider Electric\Vijeo-Designer 6.2\"
When applied, v6.2 SP9 and SP10 will move the installation folder to "C:\Program Files (x86)\Schneider Electric\Vijeo 6.2.9\"
When applied, v6.2 SP11 and SP12 will move the installation folder to "C:\Program Files (x86)\Schneider Electric\Vijeo 6.2.11\"