Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the difference between the SF6 technology and the Vacuum technology used in Schneider Make MV Circuit Breaker.

⚠ CAUTION ⚠

The information provided in this FAQ being considered as confidential content, as it can be exclusively used internally.

This flag has been added automatically when the article is published with internal visibility only.

SF6 and Vacuum are the two modern breaking techniques in the field of Medium Voltage. Refer the below table for the comparison of these two technologies:

Protection & Switching of:VacuumSF6
Breaking medium Checkingnoyes
Failure rate (MTBF)target as SF64 / 10000 units per year
Sealed for lifeyesyes
Maintenancenono
Life time30 years30 years
Mechanical Endurance10000 operations10000 operations
Electrical Endurance50 to 100 operations @ Isc20 to 50 operations @Isc
Overheads Line Transformer(IEC E2 class possible higher TRV)(IEC E2 class possible higher TRV)
MotorCircuit Breaker Contactor + protectionCircuit Breaker Contactor
Capacitor Bank(IEC C1 class : low probability of restrikes)(IEC C2 class : no reignition, no restrikes)
Arc FurnaceCBCB
CB + protectionCB + protection