Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the frame sizes of ATV61 and ATV71 drives?
Issue:
Frame sizes for ATV61 and ATV71

Product Line:
ATV61 ATV71 Altivar drives

Environment:
All

Cause:
n/a

Resolution:
See Attached Chart and use the Engineer Frame column based on the part number of the drive.

Schneider Electric Nigeria

Attachment(s)
Frame sizes atv61_71_framesizes_iv.xls [29 KB]