How can we help you today?

How to check the network by the PING command

On your PC, select the Window's [Start] button → [All Programs] → [Accessories] → [Command Prompt].
In the Command Prompt, enter "ping (the destination IP address)" and press ENT key.

PING Terminal Window

If it shows "0% loss", the network is normal. However, there is some problem if it shows "100% loss". In this case, check your network environment.