Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What should the DC bus measure on an ATV312H...N4?

Issue:
How do I calculate / determine the DC bus value ?

Product Line:
Altivar 312

Environment:
All Altivar models and serial numbers

Cause:
Input rectifiers or DC bus have failed

Resolution:
The value of the DC bus voltage is dependent on the supply voltage.  The DC bus voltage should be approximately the value of the peak line supply voltage.  Example:  If the line supply voltage measures 480vac (RMS), then the DC bus will be 480 X 1.414 or approximately 678Vdc.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings