Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Do we have replacement cooling fans for the FLEX58 drives?

Article available in these languages: Spanish

Issue:
Do we have replacement cooling fans for the FLEX58 drives?

Product Line:
Econoflex Flex58

Resolution:
Reference bulletin number 30072-450-46

*Fan kit 31158-296-50:  Flex58KU90N4, Flex58kD12N4, Flex58KD16N4, Flex58KD23N4, Flex58KU90M2, Flex58D12M2 ( Fan voltage is 120vac)
*Fan kit 31158-296-51:  Flex58KD28N4, Flex58KD33N4, Flex58KD46N4, Flex58D16M2, Flex58D23M2  (Fan voltage is 12vdc)
*Fan kit 31158-296-52:  Flex58KD54N4, Flex58KD64N4, Flex58D28M2, Flex58D33M2, Flex58D46M2  (Fan voltage is 12vdc)

No fan kit required:  Flex58KU18N4, Flex58KU29N4, Flex58KU41N4, Flex58KU54N4, Flex58KU72N4.

*Please note these fans are no longer available for sale and are obsolete with no direct replacement. Customers should consider upgrading to the current designs of drive products to suit the application.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Nigeria

Attachment(s)
30072-450-46.pdf [2.08 MB]