Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to write a script to open a popup window in Vijeo Designer

Issue

How to write a script to open a popup window in Vijeo Designer

Product Line

Vijeo Designer

Resolution

Below is the syntax to open a popup window using a script in Vijeo Designer:

Window1.open(80,100);   // Window1 is the Popup Window Name and 80,100 are the x,y coordinates

Window1.changePanel(10010);   // Window1 is the Popup Window Name and "10010" is the panel number

Window1.show(true);  // // Window1 is the Popup Window Name