Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can you use the ATV71 main control board on the ATV61 drives?

Issue:
ATV71 MCB compatible on the ATV61?

Product Line:
Altivar ATV61 and ATV71

Environment:
All

Cause:
Can you put an ATV71 main control board on the ATV61 to make the ATV61 drive to become an ATV71?

Resolution:
No, you can not use the ATV61 main control boards on the ATV71, and you also can not use the ATV71 main control board on the ATV61.

These boards are not to be interchanged.