Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can I check fault time on an Altivar 61/71 Drive?

Issue:
ATV61/71 Fault time check

Product Line:
ATV61/71

Environment:
All serial numbers for ATV61/71

Cause:
Fault time

Resolution:
The drive does not have a real time clock to show fault time of the day.  It will only show you the drive's elapsed time during the fault.  You can then compare to the 'Run Time' shown in the Drive Menu under 1.2 Monitoring.
To navigate to Fault History:
Go to Drive Menu > 1.10 Diagnostics > Fault History