Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What can cause an error code EPHO on the ATV21 and ATV212 (also S-Flex) drives?
Issue:
ATV212: EPHO or output phase loss fault

Product Line:
ATV212, ATV21, S-Flex

Environment:
All models and serial numbers

Cause:
Motor may not be connected.

Resolution:
Check that the motor is connected to the drive.
If the unit has a bypass option you will have to deactivate the output phase loss protection by setting F605 to 0.

Link to ATV212 Programming manual
https://www.se.com/ww/en/download/document/S1A53838/