Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How many 0U accessory channels (RCC's) are included with NetShelter SX cabinets, and how manu PDUs can fit into them?

Issue:
Customers need to know how many 0U accessory channels are in each cabinet, and how many PDUs can mount into them.

Product Line:
NetShelter SX

Environment:
All versions and serial ranges.

Cause:
Customers need to plan installation of PDUs and cable management.

Resolution:

  • All 1070 mm deep NetShelter SX cabinets have 2 0U accessory channels.
  • All 1200 mm deep NetShelter SX cabinets have 4 0U accessory channels except the Networking cabinets.
  • All 1200 mm deep NetShelter SX Networking cabinets (AR3340 and AR3347) have 2 0U accessory channels.
Each 0U accessory channel can accommodate two (2) full height PDUs.
  • A 1070 mm deep cabinet can mount up to 4 full height 0U PDUs.
  • A 1200 mm deep cabinet (except AR3340 and AR3347) can mount up to 8 full height 0U PDUs.
  • All NetShelter SX and SX Networking cabinets offer 0U accessory channels as a