Issue:
Removing the main control board on the ATV61/71 drives.
Product Line:
Altivar ATV61/71 drives
Environment:
All
Cause:
Needs to understand how to remove and reinstall the MCB on the ATV61 and ATV71 drives
Resolution:
The document number for the Instruction Bulletin on the ATV61/71 Control Board Kits is 30072-451-86A (attached below).
Released for: Schneider Electric Nigeria