Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which accessories/environmental sensors are compatible with my APC Network Management Card (or devices with embedded Network Management Cards)?


Issue

Which accessories or environmental sensors are compatible with my Network Management Card (or devices with embedded Network Management Cards)?


Product Line

  • Network Management Card 1 - AP9617, AP9618, AP9619

Devices with an embedded Network Management Card 1 include (but are not limited to): Metered/Switched Rack PDUs (AP78XX, AP79XX), Rack Automatic Transfer Switches.

  • Network Management Card 2 - AP9630/AP9630CH, AP9631/AP9631CH, AP9635/35CH

Devices with an embedded Network Management Card 2 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Rack Automatic Transfer Switches (AP44XX), Smart-UPS Online (with model prefix SRT).

  • Network Management Card 3 - AP9640, AP9641

Devices with an embedded Network Management Card 3 include (but are not limited to): 2G Metered/Switched Rack PDUs (AP86XX, AP88XX, AP89XX), Switched Rack                   PDU 9000 series (APDU9xx), Rack Automatic Transfer Switches (AP44XXA), Smart-UPS Online and Smart-UPS Online Li-On (with model prefix SRT and SRTL).

  • Netshelter Rack PDU Advanced
APDU10K devices with an embedded Network Management Card.
  • Network Management Card for 1-Phase and 3-Phase Easy UPS - AP9544, AP9547

​​​​

Environment

  • All serial numbers
  • All installation scenarios
  • All firmware versions (unless otherwise noted)
  • Compatibility excludes NetBotz devices

Cause

General compatibility information relating to supported accessories that can be connected to the "Sensor" or "Universal Input/Output (UIO)" ports. Please note, compatibility excludes NetBotz branded items that contain an onboard Network Management Card, such as NetBotz 200. Please refer to NetBotz sensor compatibility information.

Resolution
Refer to the table below:

Device/Available UIO PortsQuantity of Accessory Ports/TypeFirmware Application NameAccessories/Sensors Supported
AP96170any
  • no Universal Input/Output port(s) available
AP9618, AP96190any
  • AP9512T or AP9512TBLK
  • AP9512TH or AP9512THBLK
AP7xx series Rack PDU0rpdu
  • no Universal Input/Output port(s) available
AP77xx Rack ATS0ats, g2ats
  • no Universal Input/Output port(s) available
AP9630 or AP9630CH0any
  • no Universal Input/Output port(s)available
AP9631 or AP9631CH2/ Universal IOany
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9810 Dry Contact I/O Accessory
AP8xx series Rack PDU1/ Universal IO
1/ RJ-12 Serial
rpdu2g
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • RJ-12 Serial Port only: RF Code (Third Party) R170 Sensor Tag, requires rpdu2g v6.0.9 and higher
AP44xx Rack ATS0ats4g
  • no Universal Input/Output available
Smart-UPS Online (with model prefix SRT, available mid-late 2014)1/ Integrated UIOsumx
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9810 Dry Contact I/O Accessory
AP96400any
  • no Universal Input/Output port(s) available
AP96412/ Universal IO
2/ USB ports
any
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9810 Dry Contact I/O Accessory
  • AP9834 USB Wi-Fi device
  • NBES0301 Spot Fluid sensor, 50 ft.
    • Requires firmware v3.1 or higher
AP96431/ Universal IO
2/ USB ports
any
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9810 Dry Contact I/O Accessory
  • AP9834 USB Wi-Fi device
Smart-UPS Online Li-On (with model prefix SRTL)1/ Integrated UIO
1/ USB port
su
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9810 Dry Contact I/O Accessory
  • AP9834 USB Wi-Fi device
AP8xx series Rack PDU1/ integrated UIO
1/ RJ-12 Serial
rpdu2g (NMC3)
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9834 USB Wi-Fi device
NOTE: Rack PDUs with NMC3s (firmware v1.x.x.1 or later) do not support the RF Code Sensor Tag
APDU9xx Rack PDU 9000 series1/integrated UIOrpdu2g (NMC3)
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
  • AP9834 USB Wi-Fi device
AP44xxA Rack ATS1/integrated UIOats5g (NM3)
  • AP9335T Temperature Sensor
  • AP9335TH Temperature/Humidity Sensor
APDU10K Rack PDU Advanced2/ Sensor portsapc.fw
  • APDU1300 Advanced Sensor Hub
  • APDU1308 Advanced Rope Leak Sensor
  • APDU1335T Advanced Temperature Sensor
  • APDU1335TH Advanced Temperature and Humidity Sensor
  • APDU1335T3H Advanced Three Temperature and Humidity Sensor
AP9544 (NMC 1-Phase Easy UPS)1 USB porteu1p
  • AP9834 USB Wi-Fi device
AP9547 (NMC 3-Phase Easy UPS)1 USB porteu3p
  • AP9834 USB Wi-Fi device