Issue:
A user observes that some of the captions in Webreach or Web Applications 'Diagrams' are purple, while others match the caption color set in Vista.
Product Line:
ION Enterprise 6.0.x
Struxureware Power Monitoring 7.0.x (SPM 7)
ION Enterprise 6.0.x
Struxureware Power Monitoring 7.0.x (SPM 7)
Environment:
Webreach in Internet Explorer 8. (May affect other versions of IE as well)
Webreach in Internet Explorer 8. (May affect other versions of IE as well)
Cause:
If the objects in Webreach or Web Applications 'Diagrams' have actions associated with them (Example: they open another diagram) Internet Explorer will recognize this as a link. When the customer clicks the link, Internet Explorer treats this as a visited link.
If the objects in Webreach or Web Applications 'Diagrams' have actions associated with them (Example: they open another diagram) Internet Explorer will recognize this as a link. When the customer clicks the link, Internet Explorer treats this as a visited link.
Resolution (Workaround):
In Internet Explorer, navigate to Tools> Internet Options.
On the General tab, under the 'Appearance' heading click "Color".
Uncheck "Use Windows Colors" then can change the color of the "Visited" links to match the caption color set in Vista.
In Internet Explorer, navigate to Tools> Internet Options.
On the General tab, under the 'Appearance' heading click "Color".
Uncheck "Use Windows Colors" then can change the color of the "Visited" links to match the caption color set in Vista.
Released for: Schneider Electric Nigeria