{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
ATV32 Devicenet setup configuration assistance.

Issue:
ATV32 Devicenet Programming

Product Line:
Altivar 32

Environment:
All ATV32 drives with Devicenet option card VW3A3609.

Cause:
Programming assistance

Resolution:
CONF enter
FULL enter
CON enter
CbD enter

Communications settings

AdrC= address= set 0-63
bdr= Bit rate=  Auto, 125K 250K,500K  choose one
bdrU= Data rate= Auto, 125K, 250K, 500K choose one
C1DA= Assembly set up= 20, 21, 100, unconfig  choose one
OCA1 and OMA1 are for assemblies 100 and 101 only.

See page 20 of 88 in the manual. https://www.se.com/us/en/download/document/S1A28702/

Schneider Electric Nigeria