Issue:
Why am I getting an error message: "Connection refused by server" when using Vijeo Design'Air with security?
Product Line:
Vijeo Designer, Vijeo Design'Air, Magelis
Resolution:
When enabling Vijeo Design'Air Security, the default value of the system variable _RemoteViewer.DisableConnections changes to 1, disabling any remote connections to the target machine.To allow a remote connection at run time, you can use a method (such as, a switch or an action) to set this variable back to zero.
Released for: Schneider Electric Nigeria