Issue:
ATV32 part number for the Ethernet IP/Modbus TCP/IP option card.
Product Line:
Altivar 32 series drives.
Environment:
All models, All serial numbers.
Cause:
Part number unknown.
Resolution:
The part number for the combination Ethernet IP/Modbus TCP/IP card for the Altivar 32 series drives is VW3A3616
ATV32 part number for the Ethernet IP/Modbus TCP/IP option card.
Product Line:
Altivar 32 series drives.
Environment:
All models, All serial numbers.
Cause:
Part number unknown.
Resolution:
The part number for the combination Ethernet IP/Modbus TCP/IP card for the Altivar 32 series drives is VW3A3616
Released for: Schneider Electric Nigeria