Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the control power voltage for the ATSU01 soft starter?

Issue:
Control power voltage for the ATSU01 soft starter.

Product Line:
ATSU01

Cause:
Literature is conflicting.

Resolution:
The ATSU01 uses 24VDC control power only.  It does not use 24VAC.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)