Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Err7 fault on the ATV212 drive?

Article available in these languages: Spanish

Issue:
Err7 Fault ATV212.

Product Line:
ATV212

Environment:
All serial numbers for ATV212

Cause:
N/A

Resolution:
Err7 means the motor current sensor in the drive is inoperable.  The best resolution would be to replace the drive.