Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why does the drive read RDY after the run command is given to LI1 on ATV312 drive?

Article available in these languages: Spanish

Issue:
RDY on screen after the run command is given to LI1

Product Line:
ATV312

Environment:
All

Cause:
Will not turn on motor

Resolution:
RDY on the HMI display means no run command has been issued.
Measure voltage between LI1 and com terminals verify +24Vdc is present with run command
Check the wiring between LI1 and +24Vdc ( customer switch )
Verify the programming is setup for terminal control ( CCS and Cd1 menu CtL)
Verify tCC settings for 2wire / 3wire matches the run command wiring.
Verify the drive is "not" in local mode ( push the green run button on the HMI )