Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are line reactors required for the Altivar ATV61 and Altivar ATV71 drives?
Issue:
Are line reactors required for ATV61/ATV71?

Product Line:
Altivar 61 , Altivar 71

Environment:
All models, All serial numbers.

Cause:
Product characteristics unclear.

Resolution:

Our 208/230 and 400/480V rated Altivar 61/71 drives do not require line reactors.  However, depending on the voltage and power quality of the incoming power, a line reactor or other power conditioning device may be necessary in a given installation.  Line reactors are used to filter and clean noisy power being fed into the drive.  They also can lower the incoming voltage a few percentage points if your incoming voltage is running a little high so they are used on a case by case basis, as needed.

The ATV61/71 drives 100HP and below have an internal DC choke which handles a lot of the filtering and power conditioning.  Drives rated 125HP and above have an external DC choke that ships separately and must be field installed.  There is an option to use a 5% line reactor instead of this DC choke so in this case, a 5% line reactor would be mandatory on those drives 125HP and above if the customer decided to not use the DC choke. Either the DC choke or the 5% line reactor must be used, but not both.

Altivar 61/71 drives rated at 575/690V 125HP and above require a 5% line reactor also, it must be used on these drives.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings