Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is PM800 series meter RoHs Compliant?

Yes, PM800 series are RoHs Compliant. The RoHs compliant documents are attached below for PM820, PM850 and PM870.




Schneider Electric Nigeria

Attachment(s)
PM820_RoHs.pdf [88.68 KB]
PM850_RoHs.pdf [88.45 KB]
PM870_RoHs.pdf [89 KB]
PM800_RoHs.pdf [382.11 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: