Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How can you program the ATV61 and ATV71 drive to start stop with the HMI and use AI2 for 4-20mA speed control?

Article available in these languages: Spanish

Issue:
Configuration the ATV61 and ATV71 drive to start stop with the HMI and use AI2 for 4-20mA speed control.

Product Line:
Altivar ATV61 ATV71

Environment:
All

Cause:
Wants to start and stop the drive with his remote keypad display and use his 4-20mA signal for speed control.

Resolution:
Program the drive as follows
Drives MENU
Simply Start Menu 1.6
Ref 1 channel is AI2
Profile is set to SEP ( Separate)
CMD switching set to Channel 1 active
CMD channel 1 set to HMI

Schneider Electric Nigeria

Attachment(s)
ATV61 Prog Jun 07 1760649.pdf [6.84 MB]