How can we help you today?

How to test communication between Citect and equipment connected (PLC and controller in Modbus eurotherm) ?

There are two possible solutions :
1- Use ModNet native protocol has Vijeo Citect (Modbus TCP or series) .
2- Using the OPC Server through Schneider OFSOPC driver (Modbus TCP or series based on the configuration of the alias) .

Schneider Electric Nigeria