Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are fuses included with the Powerlogic Energy Meter?

Issue:
The user would like to know if fuses are included with the meter when purchased

Product Line:
Energy Meter

Environment:
Protective Fuses

Resolution:
Fuse Packs/Fuses are not included with the Energy Meter.
The fuses are typically provided by the installer or can be purchased as an accessory called fuse packs.
The fuse packs come with 1/2 A SLO-BLO rating and can be ordered in packs of 1, 2, or 3.

Below are the part numbers for the fuse packs.
EMFP1 Energy Meter Fuse Pack, Set of 1 (includes 1 fuse)
EMFP2 Energy Meter Fuse Pack, Set of 2 (includes 2 fuses)
EMFP3 Energy Meter Fuse Pack, Set of 3 (includes 3 fuses)

Diagram

Schneider Electric Nigeria

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: