Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Why do I see 115 VAC on the outputs of the BMXDAO1605 when there is no load connected to to module?

Issue:

Why do I see 115 VAC on the outputs of the BMXDAO1605 when there is no load connected to to module?

Product Line:

BMXDAO1605

Resolution:

This is normal when attempting to measure a triac output with no load.  Triac outputs cannot be accurately tested without a load.
The high impedance of the voltmeter will introduce enough of a load to cause the applied voltage on the triac to be seen.
Test with a load applied to the triac and you'll get a more meaningful measurement.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)