Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What are the replacement CT's or current transformers for the ATS48C66Y soft starter?
Issue:
What are the replacement CT's or current transformers for the ATS48C66Y soft starter?
Product Line:
Altistart ATS48
Environment:
All
Cause:
Replacement parts needed.
Resolution:
CT's are part of the bus bar assembly VZ3N005S48 however this part is not available to purchase. One option is to return the Soft Start for repair.