Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
In programming PID, what does parameter FbS do on an ATV312 drive?
Issue:
Parameter FbS (feedback scale factor)

Product Line:
ATV31 and ATV312

Environment:
All models and serial numbers

Cause:
None

Resolution:
The parameter FbS is a parameter that can be used to scale the reference according to the range of the feedback sensor.
Example: Regulating pressure
PI reference range of process, 0-50 psi (0-100%)
Range of pressure sensor, 0-100 psi
FbS = Max sensor range / Max process range
FbS = 100/50 = 2

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre
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
  • Legal Information
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings